เลือกตำแหน่งที่ตั้งของคุณ:

ประเทศ

กรุณาเลือกภาษา:

Machine loading intelligently automated: Experience KUKA at EMO 2023

When the leading global trade fair for production technology, EMO, opens its doors in Hanover from September 18 to 23, 2023, KUKA will be there. In keeping with the motto “industrial intelligence in automation_maximum performance for machine tools", we will be presenting innovative robot and software solutions that make companies more productive and sustainable and help to defy the shortage of skilled workers.


Load machine tools intelligently and precisely

Machine loading, deburring workpieces, cleaning them or finishing them – these are important tasks that hardly anyone wants to do anymore. Because on the one hand, they require speed and precision, and on the other hand, the tasks are monotonous, repetitive and physically demanding. Industrial robots, mobile robotics and other automation solutions from KUKA reliably relieve human teams of many tasks related to machine loading. EMO visitors can experience exactly how in Hall 9 at Booth D42.

The MAIROFlex iisy modular automation cell reliably loads a wide variety of machine tools with components and does not require a safety fence.

KUKA Highlights at EMO 2023

  • Mobile robotics

    Product: Mobile platform KMP 1500P, mobile cobot KMR iisy and automation cell MAIROFlex iisy, presented at the "Mobility Area"

    Applications: Machine tool loading and unloading, transport of components

    Advantages: optimal utilization of the production area, time saving, flexibility

    เรียนรู้เพิ่มเติม
  • Future of work

    Product: LBR iisy, operating system iiQKA.OS and digital ecosystem, presented at the “Cobot Area”

    Applications: Get to know High Torque Screwing, Machine Tending, Simple Assembly and handle the LBR iisy yourself

    Advantages: easy to program, fast commissioning, collaborative and secure

    เรียนรู้เพิ่มเติม
  • Efficiency increase

    Product: KR CYBERTECH with software package KUKA.SmartBinPicking and Vision & Sensor Toolkit
    Application:
    the precise reach into the box: Bin picking of components with AI-based object recognition
    Advantages:
    singularity and collision free, relief of employees, higher productivity possible

    เรียนรู้เพิ่มเติม

Experience KUKA live at EMO

Secure your ticket for EMO 2023 at Hannover Messe now! We look forward to meeting you at booth D42 in hall 9 between September 18 and 23, 2023.

Mobile support thanks to mobile robotics

In our “Mobility Area” at EMO, you will gain insights into the possibilities of mobile robotics. Experience the HRC-capable mobile KMR iisy, which is intuitive to operate, fast and safe on the move. Get to know the KMP 1500P platform, which confidently moves up to 1,500 kilograms. And discover the potential of the MAIROFlex iisy automation cell without a protective fence, which allows machine tools to be supplied and loaded flexibly as never before. Its small footprint, simple installation and attractive cost-benefit ratio make the MAIROFlex iisy attractive for small and medium-sized companies, among others.

Logistics on a new level: The mobile Cobot KMR iisy and the KMP 1500P (right) make it possible.

Component removal from boxes – fast, collision- and singularity-free

Last year, the software product KUKA.SmartBinPicking celebrated its premiere, and now it is supporting international companies in production. Based on KUKA's outstanding robotics and path planning expertise, the KR CYBERTECH confidently and precisely reaches into the crate and feeds components for further processing. Experience for yourself how the robot moves collision-free in the crate with AI-based object recognition and acts with the robot hand extremely close to the component, so that the robot flange does not require an extension.

In what order and at what speed does the robot pick up the components, where does it transport them? Find out at EMO!

Gain even more detailed insights with KUKA.Sim and VDMA UMATI

The KUKA.SmartBinPicking software builds on proven functionalities of the KUKA.Sim simulation environment and also makes the 3D function modules efficiently usable for the KUKA path planner within a consistent operating concept. Another exciting feature: with the aid of a VDMA UMATI dashboard, trade fair visitors can gain an insight into the production data. Thanks to an interface, UMATI displays data on the OEE (Overall Equipment Efficiency) of machine tools in the dashboard. UMATI stands for simplified, secure data exchange between machines, components and systems - for the transparent, efficient production of tomorrow.

Strong support for your production: KUKA.PLC mxAutomation

Thanks to KUKA.PLC mxAutomation, KUKA robots can be effortlessly integrated into existing operating concepts and programmed without any special robot programming knowledge.

At the KUKA booth at EMO, visitors can experience software that makes production easier and more efficient. For example, the KUKA.PLC mxAutomation interface, which enables external controllers to command KUKA robots with all basic motion commands. Robot and machine control merge – this makes it possible to integrate KUKA robots effortlessly into existing operating concepts. Programming and adaptation of programs and robot positions can be implemented by an operator using their familiar machine language. This means that no special robot programming knowledge is required. Discover the possibilities for your company.

Robotics in the service of sustainability

Energy-efficient robots, robot controllers and systems can drastically reduce companies' energy consumption. At EMO, KUKA is presenting examples of how this can be achieved: with the aid of the robot controllers KR C5 and KR C5 micro and the latest generations of our robots. With their slim design and comparatively low weight, they consume significantly less power than their predecessors. Our automation solutions for warehouse logistics allow optimum utilization of the available space, automated guided vehicles or mobile robots – which also helps to save resources. In addition, simulation with KUKA.Sim helps to optimize processes from the outset in terms of sustainability and to reduce cost-intensive times on the construction site.

On the way to a smaller carbon footprint and climate-friendly technologies with KUKA

At EMO, we present proven solutions and innovations that make your production more efficient and sustainable. Discover the potential of fenceless mobile robotics, watch a robot doing bin picking and try out our Cobot LBR iisy. We look forward to exchanging ideas with you!

Steffen Günther, Key Technology Manager Machine Tool Automation, KUKA Deutschland GmbH