Select your location:

Location

Spoon-fed

To distribute baby-food measuring spoons quickly, system integrator MODU System in Malaysia opted for a KR DELTA from KUKA. The Hygienic Machine version of this high-speed robot is ideal for its task – and the KR DELTA can do much more.


Increased hygiene requirements, sustainable solutions

Hygiene is fundamental to food safety, and It's also a challenge in the food industry, with increased requirements for production areas, cleaning and disinfection of surfaces and equipment, and trained and healthy staff. Malaysian system integrator MODU System supports food producers with expertise in robot-based automation solutions – and assistance from KUKA, which offers the ideal robot for these requirements, the KR DELTA. “We want our customers to have confidence in us,” said Rajinderjit Singh, Regional Manager of MODU System. “That’s why we have invested considerable resources in technology development and work closely with partners like KUKA to find a more sustainable solution for robotics.

Robot spoon picking system

Peek behind the scenes at MODU System and see how the KR DELTA excels in hygienic food production applications

Pick and place: it’s a scoop!

In Klang, west of Kuala Lumpur, two KR DELTA robots pick up measuring spoons from a conveyor belt and place them on a second belt in open conveyor pockets, each holding a food bag with baby food. In a free area next to each bag, a sticker includes a bar code. “When the robot detects the free area via the camera, it knows to place a spoon there,” said Singh. Another machine then pushes the bag and spoon into a box. To avoid machinery jams during packing, the robot doesn't place a spoon if the food bag covers the sticker. What sounds relatively simple actually represents the hand-in-hand interaction of various systems in ongoing production.
The KR DELTA places the spoons next to the bag with the baby food. The next process step places both parts in their packaging

KR DELTA scores in the food industry

“Naturally, the solution centers on the KR DELTA, which can come into direct contact with food because of its stainless steel body,” explained KUKA employee Lim Jia Ming. The robot’s corrosion-resistant stainless steel housing is designed according to German LFGB andUS FDA food standards. It also meets different sets of certifications: European CE, German TÜV safety function certification and it fulfills Northamerican market access standards. The robot is protected against dust and moisture with protection rating IP 67, to support cleaning under high pressure and with alkaline or acidic cleaning agents – ideal for food-industry hygiene.

 

Perfect for food: thanks to its stainless steel housing, the KR DELTA can be used in the food industry

Up to 80 spoons per minute

With a cycle time of as little as 0.5 seconds, the KR DELTA is ideal for pick-and-place tasks. “Two robots manage about 80 spoons per minute,” said Jia Ming. At the same time, they work extremely precisely, avoiding potential manual errors. One of the biggest initial challenges for this process was accurate calibration. This is a precondition for the two KR DELTAs to grip the spoons with precision at high speed.

Before automation, the baby food manufacturer carried out this process as a potentially dangerous manual step. The Hygienic Machine version of the KR DELTA makes this a completely hygienic process – and a highly compact solution. Ceiling mounted above the assembly lines, each of the two robots occupies an installation diameter of just 350 mm.

Pick and place professionals: two KR DELTAs can handle up to 80 spoons per minute

A question of the right position

Combine KUKA.VisionTech, a powerful software package for 2D object recognition, with KUKA.PickControl, and the KR DELTA can pick up objects from one moving conveyor belt and place them on another. “One camera with image processing detects the position of the spoons on the belt, while a second detects the bags on the other conveyor. The system then calculates the distance traveled and the exact position,” explained KUKA's Jia Ming. KUKA.PickControl makes it easy to coordinate, integrate and control multiple KR DELTAs. The software also ensures a smooth and energy-efficient production sequence.
A camera detects the position of the spoons. KUKA.PickControl enables the KR DELTA to pick the spoons from the moving conveyor belt

Programming offline, testing in real time

“KUKA.PickControl supports flexible patterns, so customers can select different scenarios to pre-define and easily switch among placement patterns according to their current requirements,” said Jia Ming. In this solution, MODU System also used KUKA.Sim to check and test the customer’s specifications with a 3D simulation that transferred directly to the real controller. The intelligence of KUKA.Sim enables efficient offline programming of KUKA robots. With features such as reachability checks and collision detection, the food manufacturer could test the feasibility of the robot programs and cell layouts employed before installation.
Highly flexible, good handling: MODU System uses KUKA.Sim to ensure in advance that the application works

This robot is picky

 
Another challenge is the shape of the spoon, including its handle, which determines where the KR DELTA can grip it. “One solution is to use a dark detection area to figure out the best orientation of the spoon,” said Rajinderjit Singh of MODU System. Testing showed only a few acceptable orientations for order picking. If the orientation falls outside the specified settings, the robot ignores the spoon and grips another one. “This enables us to improve the robot's cycle time still further,” explained Singh.
Even overlapped spoons are not a problem thanks to filter settings that simply ignore them

Spoon filtering made easy

Image processing also can cope with overlapping spoons, which makes the filter setting one of the most important aspects of the application. For example, the radius filter detects and ignores overlapping spoons within an area. As Jia Ming explained, “Think of it this way: the first robot picks up the top spoon, but the bottom one is misaligned. With this filter function, the second robot ignores the spoon in question.” An elevator in front of the assembly line, followed by a vibration unit that optimally separates the spoons, helps avoid this scenario and simplify robot processing.

 

A vibration unit makes it easier for the robot to handle the spoons

The system is very easy to operate, looks good, and the stainless steel robot design convinced our food-industry customer. I am very satisfied with the automation.

Rajinderjit Singh, Regional Manager at MODU System

Blue, green or orange: spoon color does not matter

All the measuring spoons are the same shape, but the customer uses blue, green and even orange ones. These varying colors presented a further initial challenge. “For example, if the customer uses a blue spoon, red light is ideal for the vision system to detect spoon position. A combination of lighting colors shortened the image processing time,” said Singh. RGB lighting easily accommodated this setup.

A final inspection camera monitors the entire process. “The customer has great confidence in the automation solution that KUKA and MODU System have developed,” Singh explained. “We ourselves are very impressed with the stainless steel design of the KR DELTA and believe that the application is ideally suited to the food industry, which places great emphasis on hygiene.”

Find KUKA system partners in your area

Find the right partner for your industry or specific challenge here.

You might also be interested in