The KR CYBERTECH nano ARC sets the pace in automated production
Within the new generation of the KR CYBERTECH nano series, KUKA is now also presenting the specialists for continuous-path applications such as arc welding, adhesive bonding or sealant application: the KR CYBERTECH nano ARC family. In the low payload category, the robots deliver maximum performance at minimal costs.
23 Tháng Tư 2021
Lowest maintenance requirements in the low payload category
Small footprint, wide range of possibilities
High path accuracy: best results right from the outset
“We have developed the series specifically for the latest KR C5 controller generation from KUKA, which taps the full potential of our new overall system,” says Markus Hollfelder-Asam, Portfolio Manager at KUKA. “Integration of the KR CYBERTECH nano is really easy for companies thanks to the standardized mounting surfaces for accessories and identical footprint to that of its predecessor.”
The product series also features – as standard – protection against dust and water in accordance with IP 54 for the hollow-wrist robots and even IP 65/67 (main axes/wrist axes) for the in-line wrist robots.
No matter what tasks you use the latest-generation KR CYBERTECH nano ARC for, it offers outstanding results right from the outset and can be optimally adapted using the flexible KUKA.Motion Modes.