Chọn vị trí của bạn:

Địa điểm

Fragile load: KUKA palletizer for chicken eggs

Farmers around the world automate egg palletizing with Meggson. The Dutch company designs and builds robot-based systems that prepare up to 108,000 eggs per hour for shipping – and protect the health of employees.


Based in the Dutch city of Ede, the Dutch automation Meggson targets large layer poultry farms. Moving 30,000, 50,000 or even 100,000 chicken eggs per hour without breaking a single one is every bit as complicated as it is physically taxing – for farms that don't use automation. “Until a few years ago, packing and palletizing eggs was a purely manual task,” said Gijs Thomassen, Director of Meggson. “In 2009, a customer observed us carrying out this work and asked if it could be automated.” No sooner said than done.
Meggson has implemented a compact palletizing system for eggs that uses a KR QUANTEC robot. The robot can handle different types of egg containers

From purely manual labor to a compact palletizing system

Founded in 1997 as a mechanical engineering company called Cobot Automation that supplied equipment to numerous farmers and increasingly specialized in poultry farms, Meggson developed its first automation solution to handle raw eggs – with great success. As a result, the Dutch company won over customers throughout Europe, Turkey and the USA – and increasingly incorporated KUKA robots into its automation solutions. Since May 2021, the company's new name – Meggson – has matched its specialization, because eggs are its main focus.

Palletizing system provides relief for employees 

The weight of a chicken egg ranges from under 53 grams (weight class S) to more than 73 grams (weight class XL). A pallet can hold up to 10,000 eggs, so employees handle the typical transport containers for 30 chicken eggs (pulp egg trays or plastic setter trays) in stacks or layers. These weigh an average of 7.5 kilograms and must be transported, arranged and secured on a pallet at considerable speed. Meggson's Gijs Thomassen called it “tough physical work that is repeated over and over again.” Back pain and other musculoskeletal disorders are often the result. A KUKA palletizer never tires of such processes – and carries out the work quickly, efficiently and extremely gently. It is also suitable for tight, irregular spaces in which linear systems for transport and palletizing do not fit.
Into the case, onto the pallet: the KR QUANTEC exercises great care in its handling work

Palletizer scores high with special gripper

In addition to other systems it develops in house, Meggson offers automation solutions that feature a KR QUANTEC robot with a special gripper at their core. The KUKA palletizer – compact enough for an extremely flexible cell design – stands out for its precision and reach. Its grippers can handle diverse materials, including cardboard, pulp and plastic. The eggs are palletized as successfully as empty setter trays or pulp trays are loaded onto transport trolleys or placed on a conveyor belt. The robots use laser sensors to detect where they can pick up their respective loads.
Smart palletizing technology for poultry farmers: the grippers are designed to handle materials such as cardboard and plastic

Up to 108,000 eggs per hour

The Meggson ROBOT TP300 automation solution can arrange up to 108,000 eggs per hour on pallets while placing the empty containers on a conveyor belt during the process. From here, the containers are transported away – either to be discarded or to be cleaned and refilled, depending on their condition. But Meggson automation solutions can do even more. Among other things, they impress in loading and unloading egg packing machines, palletizing cases full of eggs and handling setter trays. Moreover, they are compatible with all types of egg packing machines.

The automatic system with palletizer meets the requirements of farmers in Europe, Turkey and the USA

“If the farmers are happy, so are we”

For its flexible, high-performance palletizing systems, Meggson always has relied on KUKA robots. The integrator wants to provide the best possible support for farmers, and the 20 Meggson employees, in turn, feel optimally supported by KUKA. “That is the proverbial German quality,” Gijs Thomassen emphasized. “KUKA makes the best robots while also bringing many years of know-how – and that strengthens our trust in KUKA.”

“Working with KUKA palletizers is easy,” added Gerwin van de Geer, Product Manager at Meggson. “The first automation solution for eggs was still relatively complex to program. But once everything was up and running, we were able to replicate it time and time again.” The robots work with the KUKA KR C4 controller and after a brief introduction, customers usually can run it themselves. “KUKA designed a perfect program that our farmers can use comfortably,” van de Geer stressed. “That’s why they’re very interested in working with a system from KUKA. And if the farmers are happy, so are we!”

Simplifying strenuous processes thanks to a palletizing system

One of these satisfied customers is the Salomons Group, based in the Netherlands in the town of Dronten. Currently, more than 120,000 laying hens live on the Group’s associated farms. Since March 2020, the Group’s largest free-range farm has used a customized version of the ROBOT TP300 system. An employee checks and sorts fresh eggs from the coop so only intact ones end up on the conveyor belt. From there, the eggs are automatically arranged in egg trays. Via a conveyor belt, the egg cartons also reach the KR QUANTEC robot (type KR 120 R3100-2) in its cell. With its wide, stainless steel gripper, the KUKA robot picks up 12 full egg trays at a time in one fluid motion – three layers of four trays with 30 eggs each – and the layer palletizer carefully places them on the pallet. The entire process lasts 30 seconds, and the robot performs this step three times to complete one layer of the pallet.

Efficient packing, high flexibility and fully automatic palletizing: the KR QUANTEC can handle twelve full egg trays at once

Automatic palletizer – a sensitive powerhouse

The KR QUANTEC then places a separating layer on the eggs to secure the fragile cargo. Six layers of eggs – 6,480 in all – fit on a Salomons pallet. Between steps, the KR QUANTEC automatically moves empty egg trays to a second conveyor belt. From there, they can be transported out of the room and prepared for reuse.

In total, the system prepares 36,000 eggs for shipment each hour – and does so with maximum reliability and minimal risk of breakage. In the past, two to three employees worked in unison here to load pallets. Now, one of them has taken over quality control, and the others have found less physically demanding tasks on the poultry farm.

The KR QUANTEC robot simplifies cell planning – with a streamlined in-line wrist and a small footprint

No egg is lost

“We at the Salomons Group love to find solutions that simplify processes,” stated Klaasjan Salomons, Managing Director of the family-run business. Salomons also notes that the company used KUKA palletizing robots and enjoyed working with Meggson even prior to its most recent automation project. However, Klaasjan finds that the new palletizing system does even more. For one thing, Salomons appreciates that “when a coop is changed, the leftover eggs that do not completely fill a tray can be stored temporarily on the pallet. These are then transported onward the next day.” No egg is forgotten or lost.

Working with KUKA palletizers is easy. The first automation solution was still relatively complex to program. But once everything was up and running, we were able to replicate it time and time again.

Gerwin van de Geer, Product Manager at Meggson

Scope for innovation and expansion

In an expansion phase, The Salomons Group is building a facility in Ghana, where chicken eggs are very expensive. For many people in Ghana, a professional layer poultry farm represents the chance to feed their families. The team at Meggson is happy to help free up resources for entrepreneurs like the Salomons family so they can plan and implement projects like these. For Gijs Thomassen, this is an incentive to keep developing his own automation solutions for layer poultry farms. This is because “they improve working conditions for employees and, at the same time, enable better control of egg palletization – which increases output quality.”

Bạn có cần trợ giúp để tự động hóa ứng dụng của mình không? 

Liên hệ với chúng tôi, chúng tôi sẽ sẵn lòng tư vấn cho bạn và cùng nhau tìm ra giải pháp phù hợp.

Whitepaper khuyến khích sự thèm muốn tự động hóa trong ngành công nghiệp thực phẩm

KUKA đã cung cấp các giải pháp cho hơn 1.000 khách hàng trong ngành thực phẩm và biết rõ nhu cầu cũng như thách thức của họ. Với các thành phần chất lượng cao - rô bốt, phần mềm, dịch vụ - trong sách trắng này, KUKA hiện cung cấp các công thức nấu ăn đảm bảo thành công cho toàn bộ chuỗi quy trình. Từ giao hàng đến phân phối, cho nhiều ngành công nghiệp khác nhau. Tám ví dụ thực tế cung cấp một cái nhìn sâu sắc ấn tượng.

Khám phá các giải pháp tự động hóa mà mọi người đều thích.

Tải sách trắng

Find KUKA system partners in your area

Find the right partner for your industry or specific challenge here.

Bạn cũng có thể quan tâm đến