Sustainability report
With an annual sustainability report, KUKA informs its stakeholders about approaches and measures as well as data and facts concerning sustainabilty.
현재 이전 브라우저 버전의 Internet Explorer를 사용하고 계십니다.
최적화된 보기를 위해 브라우저를 업데이트해 주십시오.
With an annual sustainability report, KUKA informs its stakeholders about approaches and measures as well as data and facts concerning sustainabilty.
지속 가능한 발전과 KUKA인의 건강을 보호하기 위해, 우리는 건축 현장 등에서 직원의 안전을 보장하는 품질경영시스템을 도입하였습니다. 여기에는 전반적인 보건 경영도 포함되어 있습니다. 현재 우리가 보유하고 있는 인증서는 다음과 같습니다.
This British standard is the basis for the certification of management systems for occupational health and safety. OHSAS 18001 deals with the hazards and risks related to occupational health and safety.
The health and safety accreditation system CHAS is a certification scheme for the construction industry. It serves both purchasers and suppliers as a means of assessing the health and safety competence of a company.
ISO 45001 describes requirements for an occupational health and safety management system and instructions for implementation.
우리의 환경 경영 시스템 및 에너지 경영 시스템 아래, 우리의 활동과 제품 및 서비스의 방법, 범위, 영향이 적정하도록 노력하고 있습니다. 그래서 우리는 이러한 경영 시스템을 부단히 개선하고 환경 오염을 피하고자 합니다. 이 분야에서 우리가 보유한 지속 가능성 인증서는 다음과 같습니다.
The international standard ISO 14001 defines the requirements for an environmental management system. It focuses on a continuous improvement process. ISO 14001 belongs to a set of standards which, among other things, deals with eco balance sheets, key environmental indicators as well as environmental performance evaluations.
The internationally recognized standard supports the establishment of systematic energy management as it relates to energy efficiency and CO2 emissions. KUKA has been operating an energy management system according to the ISO 50001 standard since 2016.
지속가능한 방법으로 경제 활동을 하기 위해서, 우리는 검증된 품질경영시스템을 도입하였습니다. 우리가 이 분야에서 보유하고 있는 인증서들은 우선적으로 다음과 같습니다.
This certification serves to confirm the reliable security of the international supply chain.
This set of standards deals with quality management systems and fosters mutual understanding at a national and international level.
As an automotive supplier, KUKA also has the independent VDA 6, Part 4 certification. This standard provides a means of furnishing proof that the requirements of the automotive industry are fulfilled in areas where no certification according to IATF16949 is currently possible.
This standard is intended to improve system and process quality as well as customer satisfaction. The focus is on discovering errors and deficiencies and not just preventing them.
This internationally recognized standard serves as a quality management system for the aerospace industry. EN/AS9100 is based on the ISO9001 certification.
There are also set quality management systems for the medical industry. The associated ISO13485 certification defines the requirements for the design and manufacture of medical products.
As a welding expert, this standard is also important for KUKA. It describes the quality requirements for manufacturers of fusion-welded components and assemblies.
This status allows us as a company to ship air cargo designated as “secure”.