Sustainability report
With an annual sustainability report, KUKA informs its stakeholders about approaches and measures as well as data and facts concerning sustainabilty.
Internet Explorerの旧バージョンのブラウザが使用されています。
最適な表示にするにはブラウザを更新してください
With an annual sustainability report, KUKA informs its stakeholders about approaches and measures as well as data and facts concerning sustainabilty.
持続可能な発展とKUKA従業員の健康を守るために、弊社は例えば工事現場における従業員の安全を保証するための品質管理システムを導入しています。それには徹底した健康管理も含まれています。弊社の現在の認証:
This British standard is the basis for the certification of management systems for occupational health and safety. OHSAS 18001 deals with the hazards and risks related to occupational health and safety.
The health and safety accreditation system CHAS is a certification scheme for the construction industry. It serves both purchasers and suppliers as a means of assessing the health and safety competence of a company.
ISO 45001 describes requirements for an occupational health and safety management system and instructions for implementation.
弊社は環境管理システムやエネルギー管理システムを使って、事業活動、製品およびサービスの種類、範囲、影響が適正であるように管理しています。このため、弊社は継続的に管理システム改善に取り組み、環境汚染を回避しています。この分野における弊社のサステナビリティ関連認証:
The international standard ISO 14001 defines the requirements for an environmental management system. It focuses on a continuous improvement process. ISO 14001 belongs to a set of standards which, among other things, deals with eco balance sheets, key environmental indicators as well as environmental performance evaluations.
The internationally recognized standard supports the establishment of systematic energy management as it relates to energy efficiency and CO2 emissions. KUKA has been operating an energy management system according to the ISO 50001 standard since 2016.
持続的に経済活動を行うために、弊社は定評のある品質管理システムにも力を入れています。この分野における弊社の認証は主に以下のものです:
This certification serves to confirm the reliable security of the international supply chain.
This set of standards deals with quality management systems and fosters mutual understanding at a national and international level.
As an automotive supplier, KUKA also has the independent VDA 6, Part 4 certification. This standard provides a means of furnishing proof that the requirements of the automotive industry are fulfilled in areas where no certification according to IATF16949 is currently possible.
This standard is intended to improve system and process quality as well as customer satisfaction. The focus is on discovering errors and deficiencies and not just preventing them.
This internationally recognized standard serves as a quality management system for the aerospace industry. EN/AS9100 is based on the ISO9001 certification.
There are also set quality management systems for the medical industry. The associated ISO13485 certification defines the requirements for the design and manufacture of medical products.
As a welding expert, this standard is also important for KUKA. It describes the quality requirements for manufacturers of fusion-welded components and assemblies.
This status allows us as a company to ship air cargo designated as “secure”.