Select your location:

Country

KR QUANTEC PA palletizes faster than ever

The most powerful palletizing robot on the market is getting even faster: The second generation of the KR QUANTEC PA features an impressive reduction in cycle times. With a payload of up to 240 kilograms and food-grade NSF H1 lubricants, this robot is a real asset for the food industry.

January 26, 2022


Even faster, even better: Automation specialist KUKA has completely reworked its KR QUANTEC PA. Developed specifically for demanding palletizing tasks, this second generation design, released in October 2021, includes optimized weight and center of gravity as well as improved drive units, which build on the latest technology for gear units and motors. Its reduced footprint requires very little space. Up to 10% faster that its predecessor with a comparable payload, the KR QUANTEC PA also sets new automated production standards for cycle times.

Performance redefined

“With the second generation of the KR QUANTEC PA, we have achieved a perfect balance between axis velocity and accelerationfor the best cycle times,” said KUKA product manager Michael Laub. For example, the robot type achieves 28.3 cycles per minute with a payload of 240 kilograms. “Beyond this, we also worked to increase axis velocities – for example, for layer formation during palletizing or long 180° rotations.” To meet the increased requirements of the consumer goods industry, especially the food industry in the secondary sector, KUKA also offers the palletizing robot in a “Hygienic Oil” (HO) variant. which uses food-compatible NSF H1 lubricants in all axes and the energy supply system. 
Suitable for the food industry: the KR QUANTEC PA HO with H1 lubricants in all axes
New generation, more power: The KR QUANTEC PA palletizing robot boasts world-leading speeds

Sustainably cost-efficient

Standard KR QUANTEC PA models and their HO variants are designed for the latest KUKA KR C5 robot controller. These second-generation robots also offer outstanding value and total cost of ownership (TCO). The Mean Time Before Failure (MTBF) of the entire robot arm has improved significantly to 400,000 hours while maintenance effort has reduced by 50% compared to predecessor models. With this new design, the robot only needs a visual inspection, lubrication of the counterbalancing system bearings and an oil change every 20,000 operating hours. This likely makes the KR QUANTEC PA the best robot in its class.

Innovative cell concepts for palletizing tasks

“A KR QUANTEC PA is a sustainable investment in the future of production,” said Michael Laub. “In conjunction with the KUKA.PalletTech technology package, the robot enables innovative cell concepts for palletizing tasks, particularly for the consumer goods industry.” Here, maximum performance meets minimum programming effort – for extremely fast start-up.
Different packing patterns and stations are no problem for the KR QUANTEC PA with the KUKA.PalletTech software