![Der KUKA flexibleCUBE wird mittels Drehtisch neu bestückt](/-/media/kuka-corporate/images/industries/case-studies/hartan/hartan_kuka_flexiblecube_mitarbeiter_drehtisch_header.jpg?rev=-1&w=1900&hash=42BD415D40993BB5EAF2B33842D0B24B)
Automation is child’s play with the KUKA flexibleCUBE
KUKA Industries is a technology leader in the field of joining and an ideal partner where safety-relevant components are concerned. The transfer of technology from the automotive industry makes it possible to use these processes in general industry as well. In this case, it makes us a reliable partner for Hartan
The task
The challenge at hand is the weekly manufacture of 3,000 welded parts which are essential to the entire geometry, movement and stability of the baby carriage. This line must guarantee the entire production of seats and backs for the company’s nine completely different baby carriage models. The parts of the carriage which require welding are absolutely critical to safety and must be 100 percent flawless.
Due to KUKA’s many years of experience in automating joining processes, the baby carriage manufacturer opted for a flexible standard robotic welding cell from KUKA Industries. The Augsburg-based system builder has decades of expertise in joining technology and offers an automated solution which solves capacity bottlenecks, fulfills the highest quality requirements and performs intricate welding work – the KUKA flexibleCUBE.![](/-/media/kuka-corporate/images/industries/case-studies/hartan/kinderwagenhartan_k.jpg?rev=-1&w=1400&hash=495D6905CA6193722091827D6275F68D)
The solution
The arc welding cell is particularly suitable for automation newcomers, as it can be integrated into the manufacturing process easily and seamlessly. Arc welding is the ideal joining process when it comes to steel joints. The weld seam must hold up in quality control tests, since it is a question of safety-relevant parts.
This precise welding task is no problem for the KUKA flexibleCUBE.
![Roboter im KUKA flexibleCUBE beim Schweißen](/-/media/kuka-corporate/images/industries/case-studies/hartan/kukaflexiblecube_hartan_s0754__42r3524.jpg?rev=-1&w=1400&hash=1E2F453EE35222459AA9101DDDDEF738)
Advantages of the KUKA flexibleCUBE
- User-friendly thanks to plug & play functionality
- High degree of investment security
- Flexibly deployable, as the cell can be easily adapted to the manufacturing environment
- Characterized by a high level of process quality.
The KUKA flexibleCUBE is a standardized welding cell which enables simple automation in the production plant. The Cube is equipped with KUKA components on a modular basis and can be combined with service-proven welding equipment from leading manufacturers. KUKA Industries supported Hartan in the process development and recommended the optimal equipment for this task. In the end, the modular welding cell was equipped with a KR 5 arc, a power source with welding equipment, a turntable, plus a central extraction system, torch cleaner and TCP check. It is the flexible answer to the requirements of an automated welding cell.
Right from the start, we have had no problems with the cell. Unlike other automated cells at the plants of suppliers and partners, we have had no downtimes to speak of. We make baby carriages as if they were for our own children.
![](/-/media/kuka-corporate/images/about-kuka/standorte-teaser.jpg?rev=-1&w=1400&hash=46DE3118EE6D164AB6D1C616952D0D0B)