เลือกตำแหน่งที่ตั้งของคุณ:

ประเทศ

กรุณาเลือกภาษา:

Ecological responsibility

As an industrial company, KUKA wants to make a measurable contribution to the reduction of environmental pollution. For this, we are making a start in our own company: we are cutting our consumption of energy and other resources, lowering our emissions and reducing our quantities of waste.Moreover thanks to their efficiency, KUKA robots and systems help our customers to save costs, while at the same time contributing to the conservation of resources and combating climate change.


Environmental issues (e.g. energy consumption in production, but also waste and water management) are continuously taken into account and evaluated by us. Energy consumption gives rise to CO₂ emissions. With our certified environmental and energy management systems, we ensure that negative impacts of our energy consumption are kept as low as possible and continuously minimized.

 

Energy-efficient robots and systems are an important lever for reducing energy consumption in our customers’ applications. In our own research and development as well as in cooperation with renowned partners from industry and research, we systematically address customer requirements and are continuously working on solutions with the objective of reducing consumption still further.
With technical means such as an optimized energy model in the case of newly developed robots, the upgrading of welding processes, preconfigured “ready2_use” applications and large-scale automation solutions for warehouse logistics, we have recently launched groundbreaking innovations that reduce the energy consumption of our products. In 2020, we also launched innovations that support energy-efficient production, such as the KR IONTEC, the KR SCARA and the KR C5 robot controller.

 

KUKA additionally offers customers tailored complete solutions for automating manufacturing processes, covering all activities from planning and design through

to the implementation of automated production systems. The expertise lies in automating individual production processes such as welding and joining, processing various materials and integrating different production stages to form a fully automatic system. Here, KUKA is able to offer its customers alternative energy-efficient solutions.

 

Additionally, KUKA implements automation solutions for forward-looking warehouses and distribution centers. The business segment Swisslog offers data-driven and robotbased automation from small entry-level automation systems to turnkey logistics solutions. Swisslog has created its own energy efficiency label called GreenLog for its customers. This is because energy consumption is an important criterion in complex logistics applications with many individual automated processes.

 

Noticeable savings can be achieved by improving energy management for entire plants or subsystems. For example, the power requirement peaks that occur when shuttles or stacker cranes start to move can be considerably reduced by sequencing the start times. Brake energy regeneration can also be used to reduce power requirement peaks at the start of motion. Energy efficiency gains like these can be simulated in advance, enabling customers to participate in determining their own ecological footprint in various scenarios.


Such improvements enable our customers not only to generate a competitive advantage, but also to achieve a significant improvement in their environmental performance.