Vyberte si svou polohu:

Místo

KUKA Medical Robotics team

KUKA has a special business unit focusing on medical robotics. The team offers medical device manufacturers a range of services covering research and development, sales, quality, marketing and support and can draw on almost three decades of experience in the field of medical technology.


Working in partnership 

The collaboration begins with joint workshops. In these workshops, the requirements and options relating to the planned medical device are discussed so that the most suitable system can be developed for doctors and patients. Once this has been achieved, medical device manufacturers have the opportunity to evaluate the most suitable robot for their circumstances and create a prototype of their medical solution. KUKA facilitates this process with robot training courses and a tailored technical support team. This team is also on hand during the further development of the medical device to help them configure a suitable robot, controller and software.

This tailored support during the development phase has enabled KUKA to establish itself as one of the world’s leading supplier of robotic components through its expertise. For almost 30 years now, KUKA robotic systems have been successfully integrated into the products of numerous medical technology companies worldwide.

Find out more about our business model

Development, high precision, maintenance and design: KUKA meets the requirements for the development processes of medical robots. Our customers are responsible for developing systems for medical use.

Expertise in medical robotics

  • Experience in the medical sector

    The Medical Robotics team has been marrying expertise in robotics with the requirements of medical technology for almost three decades.

  • Support during the approval process

    Drawing on our years of experience, we support our customers on their way to market through CE, CFDA and FDA approval processes.
  • Software designed for medical applications

    Specially certified LBR Med software and suitable interfaces facilitate seamless integration into medical systems.
  • Technical language expertise

    We are fully versed in specialist topics and regulatory requirements relating to medical devices and are successful at merging the fields of robotics and medicine.

Service expertise

  • Putting the customer first

    The team’s experts work with customers to develop content and processes for customized solutions that support physicians and benefit patients.
  • Quick productization

    Certified LBR Med robots and exclusive customer support enable our customers to turn a prototype into a final product quickly.
  • Holistic support

    KUKA supports medical technology companies throughout the entire life cycle of the medical device, from the initial idea to after-sales management, maintenance and service.
  • Made in Germany

    Medical products developed on the basis of KUKA robotics are characterized by high quality and award-winning design – made in Germany. 

LBR Med robot training courses

KUKA offers its customers special training courses for robots used in medical technology.

Jak udržitelná je elektromobilita?

Téma „udržitelnost“ a „udržitelná mobilita“ již nejsou tématy budoucnosti, ale mění naše spotřebitelské chování již dnes. Ale do jaké míry je elektromobilita opravdu udržitelná?

Aby bylo možné udržitelnost lépe posoudit, je v ideálním případě třeba podívat se na celý proces od těžby surovin až po recyklaci. Za tímto účelem musí být v budoucnu při plánování výrobních zařízení vyvinuta koncepce recyklace. Společnost KUKA zohledňuje celý životní cyklus produktu a poskytuje komplexní rady, jak lze zvýšit udržitelnost. Již ve fázi plánování zařízení dbáme na efektivní komponenty, které mají nejen nejnižší možnou potřebu náhradních a opotřebitelných dílů ve fázi provozu, ale také jejichž energetické nároky a náklady na údržbu jsou nízké a vykazují nejdelší možnou dobu použití nebo dalšího použití (Second-Life). Aby naši zákazníci byli optimálně připraveni na budoucnost.

  • Koncepce recyklace

    Zda second-life baterie, tedy další používání již vyřazené baterie pro elektromobily, například jako úložiště energie v soukromých domácnostech, nebo získávání cenných surovin – recyklační koncepce musí být spoluvypracovány už ve fázi plánování nového výrobního zařízení. Likvidace použitých automobilových a průmyslových baterií spalováním nebo skládkováním je zakázána a musí být zajištěno, aby veškeré staré zásoby byly zpracovány a recyklovány podle nejnovějšího stavu techniky.

  • Suroviny

    Kromě recyklace lithium-iontových akumulátorů nebo lithium-iontových baterií hraje zásadní roli i jejich výroba. V současnosti je pro výrobu baterií pro elektromobily stále ještě potřeba vzácných surovin (grafit, lithium) a vysokého energetického výdeje. Ve střednědobém horizontu však bude výzkum i zde pokračovat ve vyhledávání udržitelnějších alternativních zdrojů.

    dozvíte se více
  • Trvalá udržitelnost

    Jednou proměnnou v otázce udržitelnosti je zdroj energie. Čím více obnovitelných energií se používá ve výrobním procesu a při dodávkách energie do elektrických vozidel, tím udržitelnější elektromobily jsou. Bez ohledu na výrobní proces dochází k neustálému dalšímu rozvoji technologií akumulace, například pro ukládání přebytečné energie pomocí vodíku. Efektivně využívané zdroje s cílem dosáhnout oběhového hospodářství jsou tedy překlenutím propasti mezi ekonomickou a ekologickou udržitelností.

    Ale udržitelnost jde ještě mnohem dále. Jak udržitelná je celkově výroba, jak energeticky účinné jsou používané produkty, jak CO2 neutrální je zařízení? Společnost KUKA nabízí optimální řešení a koncepce, aby se výrobní závody přizpůsobily požadavkům budoucnosti.

    dozvíte se více
  • Klima

    Elektromobilita je v popředí ochrany klimatu a nabízí příležitost snížit závislost na palivech na bázi ropy. Přestože výroba baterií spotřebuje hodně energie, klimatická bilance při provozu elektrických vozidel je lepší než u konvenčních spalovacích motorů. Klimatická výhoda elektromobilů se zvyšuje, čím častěji se nabíjí pomocí zelené elektřiny. S dalším pokrokem ve vývoji, zejména účinnějšími výrobními procesy, vyšší hustotou energie a zlepšenou chemií článků, se klimatická rovnováha baterie může v nadcházejících letech ještě zlepšit.

    https://www.kuka.com/en-de/company/about-kuka/sustainability/ecological-responsibility

Technical service and other services

my.KUKA: Your digital customer portal for accessing robot data, medical device development requirements, spare part and robot orders, license management and much more. All of this in a single user-friendly self-service interface.

3D Virtual Showroom

Virtually experience the wide range of applications of integrated robots in medical devices.

KUKA medical robotics under the microscope