Chọn vị trí của bạn:

Địa điểm

Mobile robotic cell provides support for the loading and unloading of CNC machining centers

A KUKA KR AGILUS works in the mobile MRC flextray robotic cell developed by wbt automation GmbH & Co. KG. At DANNORITZER Medizintechnik GmbH & Co. KG, the small robot loads and unloads CNC machining centers.


Robotic cell with KR AGILUS automates pick-and-place applications

At DANNORITZER Medizintechnik GmbH & Co. KG, the robotic cell MRC flextray is used to relieve qualified specialists of monotonous loading and unloading tasks. The robotic cell was developed by integrator wbt automation and equipped with a KUKA KR 6 R900 from the KR AGILUS series. The small KUKA robot ensures that the CNC machining centers are loaded and unloaded automatically. With its flexible drawer system, the solution offers a range of advantages, thus helping to meet international demand and the increasing production requirements at DANNORITZER Medizintechnik.
Flexible and Portable Robotic Machine Loading and Unloading Solution
Watch this video to see how the KUKA KR AGILUS supports the loading and unloading of CNC machining centers.

Thanks to its flexibility, precision, speed and relatively small space requirement, the robot is the best solution for us to increase productivity.

Julian Dannoritzer, Production Manager, DANNORITZER Medizintechnik GmbH & Co. KG

Flexible robotic cell optimizes CNC milling process

Using its own docking station with integrated machine interface, the MRC flextray is positioned safely and precisely at the machining center. “Thanks to the low-friction rollers, the mobile cell can be easily moved manually to the next application area, docked and started,” explains Joachim Burkert, Managing Director of wbt. The pallets are then loaded with the blanks or semi-finished parts and fed into the robotic cell. The small KUKA robot opens the relevant drawer, removes the parts and places them in the clamping fixture. Once they have been machined, the robot places the parts back on the pallet. “The parts are accessible for inspection and various parameters can be monitored to ensure process reliability without having to interrupt the automation,” explains Production Manager Julian Dannoritzer.

The robotic cell can process up to four drawers, each with two component-specific pallets. It is thus also highly suitable for small and medium batch sizes. Individual expansions can be easily tailored to specific customer requirements.

The KUKA KR 6 R900 sixx provides maximum flexibility in the MRC flextray robotic cell.

Process and quality enhancement through robot-based automation

At DANNORITZER Medizintechnik, the robotic cell, featuring a small KUKA robot, and the milling center work together reliably. The parts count can be calculated over longer periods and the operating times of the milling center have been increased. Subsequent processes are no longer required due to the application of new milling techniques. It has consequently proved possible to streamline the process and improve the quality of the products. As a result, the company intends to incorporate further products into the automation process over the long term.

Find KUKA system partners in your area

Find the right partner for your industry or specific challenge here.