自分の現在地を選択してください:

場所

One battery pack per minute: More than 100 KUKA robots in use at FAW-Volkswagen in southern China

FAW-Volkswagen manufactures up to 300,000 battery packs per year in Fo-shan in southern China. Around 100 KUKA robots are used in production, where they weld, glue or package.

2023年5月4日


The production facility known as the "MEB Smart Factory" was built specifically for the production of the all-electric MEB platform. MEB stands for Modular E-Drive System. For the Volkswagen Group, it is a reference factory for electric vehicles and a flagship for the global automotive industry around automation, smart production and digitalization. The level of automation at the MEB factory is up to 82 percent

In the factory, welding lines for battery trays are lined up with battery packaging lines. In addition, there are testing devices and logistics. Robots from KUKA weld and glue on the automated welding line for battery cases. They are also used in the packaging of the battery packs. There, robots from the KR QUANTEC, KR FORTEC and KR titan families work together to fully automate the packaging process.

More than 100 KUKA robots weld, glue or pack in the MED Smart Factory. © KUKA Group 

The FAW-Volkswagen branch in Foshan was established in December 2011. Since then, it has been an important part of the FAW Group's development strategy in South China. In addition to four large production facilities for stamping, welding, painting and final as-sembly, the state-of-the-art MEB Smart Factory was also built here, where FAW-Volkswagen manufactures the core components of electric vehicles.

More Details

Here you will find more details about the battery pack production of FAWVolkswagen in Foshan, China.

ニュース記事をダウンロードする

PDFをダウンロードする