Medical Robotics Challenge 2.0: Apply now for the KUKA Innovation Award 2025
The new round of the KUKA Innovation Award is all about robotics ideas for the future of medicine and healthcare. The finalists can look forward to a professional appearance at a major trade fair – and €20,000 in prize money for the winner. Teams can now apply with their innovative ideas.
2024년 3월 14일
Robotics has made its way into the healthcare sector and is indispensable today. This applies to everything from diagnostics and surgical procedures on patients to therapy. The possible applications are extremely diverse.
The motto of the new round of the KUKA Innovation Award is therefore "Medical Robotics Challenge 2.0", with the focus on robotics concepts for diagnosis, rehabilitation, surgery, and many other forms of therapy. The applicants should look into the future of medicine with innovative and interactive methods to improve health and care.
Major appearance at an international trade fair
The final teams will present their concepts to an international audience of experts at a major trade fair in 2025. The jury will then select the winner of the 20,000 euro Innovation Award.