自分の現在地を選択してください:

KUKA at EMO 2019

The metal industry is always on the lookout for efficient processes and new technologies. Flexibility, process reliability, the shortage of skilled labor and digitalization are developments which are reorienting the industry. At EMO 2019 in Hanover, KUKA is presenting a wide range of solutions.

2019年8月13日


Visit us at EMO 2019: Hall 9, Booth C38

Under the slogan “industrial intelligence in automation_products and expertise for the metalworking industry”, KUKA is presenting intelligent automation concepts, powerful robot cells and Industrie 4.0 topics. The new generation of the KUKA bestseller, KR QUANTEC, for example, sets new standards for the metal industry and convinces through its quality, reliability, flexibility and cost-effectiveness. The KUKA Pre-Machining Cell is a powerful solution for foundry environments which automates machining using industrial robots. In addition, KUKA is presenting new linear robots which link production sequences to multiple CNC machines – for example, further processing systems, casting machines or machine tools.

Experience KUKA at EMO 2019

Find out further details about our trade fair applications and speak with our KUKA experts for the metalworking industry on site.