自分の現在地を選択してください:

場所

"There is a great need for action here": Robotics in nursing care

New technologies are helping us to address challenges such as the shortage of skilled workers. Could robotics also help with the highly stressed areas of health and care? We asked our experts.


Teresa Scheunert
2023年6月7日
Society
読了時間: 4分間

Robotics and artificial intelligence are making their way into more and more areas - and can provide support and take over tasks in an aging society. Is there also a trend toward using robotics in care? 

Dr. Andreas Keibel: "In general, there is a great need for new technologies in the care sector. The effects of demographic change are already visible today, as is the acute shortage of nursing staff. There is a great need for action here - also with a view to the future. The use of AI/robotics in nursing and care has been the subject of intensive international research for decades. 

When using robotics in nursing, the initial focus could be on supporting operations so that employees have more time for actual care and more budget can be shifted in favor of nursing staff. One possible application here is automated logistics, for example. This could be used to provide a wide variety of goods such as meals, consumables or even beds in a timely and accurate manner. These are the first quickly achievable areas of application that do not involve direct interaction of robotics and AI with patients or residents.
 

There needs to be a shift in the industry to fund the use of advanced technology. Financial support for equipping medical and nursing facilities with modern technology, as is the case with the Hospital Future Act, for example, are a step in the right direction here."

Dr.-Ing. Andreas Keibel, Business Development Manager Medical Robotics at KUKA.

Digitization is the basis for bringing more technology into care.

As a supplier of robots and automation solutions, KUKA is primarily active in industrial production. Are there also specific projects and applications from KUKA in the field of care and healthcare?

Dr. Andreas Keibel: "In general, KUKA's technologies help to relieve people of dangerous, monotonous, or strenuous tasks. Robotics can also provide an answer to the increasing shortage of skilled workers and demographic change. In medical robotics, KUKA offers solutions for a wide variety of medical robot applications, for the benefit of patients. One example is our sensitive lightweight robot LBR Med, which was developed specifically for medical technology. The company Life Science Robotics has used it, for example, to develop the rehabilitation robot application ROBERT, for robot-assisted therapy to mobilize patients. This robot-assisted therapy relieves the nursing staff." 

Nadine Reißner: "In addition, KUKA is also engaged in research into new technologies specifically for nursing. For example, KUKA has been working with partners to research solutions for the care sector, such as robotics support for patient logistics. The goal of the project was to relieve nurses and free up time."
Nadine Reißner is Senior UX Researcher at KUKA.

You have already indicated that not every activity in nursing can be automated. What tasks can robots cover and what is difficult?

Nadine Reißner: "In general, a distinction can be made between nursing tasks and non-value-adding activities that keep nurses from their central work. These activities include documentation and administration as well as various logistics tasks. The nature of nursing activities is that people interact with people here and social connections are established. A nurse not only hands out food and puts the tray down, but also checks the patient's condition and interacts with him or her - thus recognizing how the patient is doing. The limits are with task areas that rely on social skills, such as empathy. These interpersonal levels remain the preserve of humans. AI and robotics could provide support for logistics tasks or documentation."
Rehab robot ROBERT® mobilizes patients: Robot-assisted therapy relieves nursing staff

What new developments do you expect in the near and distant future? How will AI change care?

Dr. Andreas Keibel: "Digitization is the basis for the introduction of more technology into care. For example, AI can facilitate real-time evaluation of sensors to assess situations and environments in nursing homes, for example. This can help mobile robots move around facilities to restock shelves or keep order. AI could also help to recognize people, assess their condition and in this way relieve staff."
次の記事

こちらもチェックしてみてください