Robots are assembled and disassembled more than 90 times
By the end of his two-year Multitude Tour, the robots will have been set up and taken down more than 90 times. It happens that the stage set is dismantled in less than 24 hours and reassembled in the next concert city. This is only possible if both the robots and the entire team in the background are flexible. The KUKA subsidiary in France did most of this job behind the scenes. They advised the artist in advance, gave the whole plan the necessary structure and are now the first point of contact when the robots need servicing. Always on hand: two more KUKA robots as replacements and KUKA system partner Vendôme Robotics from Paris, which acted as integrator for the program-ming and choreography of the robots with their oversized LED screens.