Euroblech 2016: KUKA Industries is fit for Industry 4
Augsburg/Hanover, September 2016 – From October 25-29, the Hannover Fair will again be the meeting place for specialists in sheet metal forming: At Euroblech, the international technology fair for the sheet metal forming industry, KUKA Industries will also be presenting its industry expertise in hall 13 booth C194. An extensive portfolio awaits interested fair visitors: From the friction stir welding cell with single axis positioner and the KUKA flexibleCUBE with double turn/tilt positioners for components such as optics for laser welding up to the simulation and program software KUKA.Sim that demonstrates machine construction knowhow in the area of Industry 4.0.
June 17, 2016
KUKA SIM: Testing virtual processes
The customer is already able to test the deployment of equipment or application processes and optimization where applicable. "Through offline programming, various areas such as development and construction work hand in hand and already test the new work projects of the customer in the virtual world", says Siegfried Heissler division manager / Vice President ARCLAS of KUKA Industries.
"For example, the customer can start new models of production sooner." Longer idle times - between the old model and the new series will be avoided due to the virtual planning phase: The production planning already exists in the simulation and programming environment. Qualitative high-value programs are also able to be created and changed without stopping production. With the KUKA.Sim family of products, KUKA develops the optimal equipment for the individual production scenarios for your customers: KUKA.Sim Layout and KUKA.Sim Pro provide an efficient approach for the development and programming of newer production orders. "For smart production, the virtual launch plays a large role", says Heissler. The digital and real equipment will be brought together early, to secure and optimize the control program and the entire behavior of the equipment. That is why KUKA uses digital product and resource data. "We thereby are already able to test equipment by means of 3D simulations in the virtual world and achieve real production start at the customer’s site within a shorter time."
KUKA gets the customer in shape for the fourth industrial revolution, from cloud-based automated solutions to the use of virtual reality. "Regardless of the scope of the digitalization process of our customers, we are able to offer them the corresponding 4.0 solutions."
The KUKA flexibleCUBE for a dynamic production environment 4.0
KUKA friction stir welding - the technology for the growing e-mobility market
Visitors to the fair will be convinced of the level of welding expertise by KUKA. The automation professional will present a robot-based solution to achieve a three-dimensional, linear joining seam. "In combination with a single axis positioner, the orbital welded joints are no longer a challenge", says Heissler. Additionally, new process monitoring and documentation show the KUKA PCD (Process Control and Documentation) System. The process data will be numerically monitored and electronically archived and available for further possible analysis in an e.g. cloud system. That is the basis for the implementation of Industry 4.0 and accomplishes more productivity, acceptable quality and data transparency.