Chọn vị trí của bạn:

Địa điểm

The new way of building

There is a lack of affordable housing around the world. Conventional home construction cannot meet this challenge alone. KUKA is playing a decisive role in the solution with automated modular home construction.


Romy Schoenwetter
15 Tháng Năm 2024
Technology
Thời gian đọc: 2 phút

The list of advantages of automated modular construction is long. It ranges from higher efficiency and unparalleled quality to improved working conditions and sustainability in construction.

A specific example: construction time is shortened by up to 70 percent. Furthermore, the total cost is less by a quarter (compared to conventional building methods). Only the creation of the foundation and final assembly are carried out at the construction site.

KUKA is supplying the German-Austrian PropTech company for sustainable and serial construction with a turnkey and flexible system that can produce around 3500 residential units per year. © GROPYUS

Automated home construction is a key topic for the future with innovative drive, and one that KUKA is already implementing with customers – for example with a leading supplier for 3D modular home construction in England.

In 2024, for thefirst time in Germany, a flexible turnkey system will be completed in cooperation with a company for sustainable and serial construction. A special feature here is the AGV-based distribution center, which allows maximum flexibility for end customers. With a degree of automation of up to 86 percent, the new production line can produce a wall element in just 17 minutes. The infographic provides valuable insight. 

Automated modular house building

From the construction site to the factory

Bài viết tiếp theo

Bạn cũng có thể quan tâm đến