Chọn vị trí của bạn:

Địa điểm

Probably the first fast food robot machine in the world

It is small, agile and precise – and will soon be exciting fast food enthusiasts around the globe: the KR 3 AGILUS from KUKA won over the Brazilian company Bionicook and is now serving the company’s snacks, beverages and desserts to guests in the world’s first fully automated fast food machine of its kind.

06 Tháng Hai 2020


A KUKA robot at work in the restaurant business 

Industrial companies have long been relying on automation solutions with robots. However, other sectors can leverage the advantages of using machines as well. Robots for fast food restaurants? Robots in the restaurant business? In his goal of optimizing the food industry, or more precisely the fast food segment, entrepreneur Fabio Rezler from Caxias do Sul, Brazil answered these questions in the affirmative. The solution: an automated concept. The partner? KUKA. The result: Bionicook. A fast food machine where the robot cooks and serves.
The KR 3 AGILUS cuts a fine figure not only in industrial settings, but as a serving robot as well.

We are proud to have been a part of this project and to have been able to implement this idea.

Edouard Mekhalian, Managing Director of KUKA Roboter do Brasil

Food on demand – thanks to the fast food robot

Thanks to KUKA’s expertise and the KR 3 AGILUS, it was possible to work together with the Brazilian automation company AUTTOM to create the world’s first fully automated fast food counter. The concept was presented at the MIND7 STARTUP trade fair in Caxias do Sul in May 2019.

With the fast food machine, customers can choose between 14 snacks, two desserts, three salads and 15 beverages. Guests place their order via a touch panel. Once they have paid, the serving robot starts preparing the order. It autonomously handles and serves the items. To do so, it fetches the food, cooks it if necessary and serves it. The food is deep-frozen and pre-portioned. The robot serves the order within three minutes, and fills up to 100 orders per hour.

Compact design and speed: that is what the serving robot offers

It requires little space, yet is extremely agile: The properties of the KUKA KR 3 AGILUS are convincing numerous industries. It has a payload capacity of 3 kilograms and a reach of 540 millimeters. It makes it possible to achieve shorter cycle times and to increase output. An ideal basis for the fully automated fast food counter: the robot delivers meals in a minimum of time – around the clock, seven days a week.
Space-saving and flexible: these are the properties of the KR 3 AGILUS that are attracting the attention of a wide range of industries. 

Bạn có cần trợ giúp để tự động hóa ứng dụng của mình không? 

Liên hệ với chúng tôi, chúng tôi sẽ sẵn lòng tư vấn cho bạn và cùng nhau tìm ra giải pháp phù hợp.

Whitepaper khuyến khích sự thèm muốn tự động hóa trong ngành công nghiệp thực phẩm

KUKA đã cung cấp các giải pháp cho hơn 1.000 khách hàng trong ngành thực phẩm và biết rõ nhu cầu cũng như thách thức của họ. Với các thành phần chất lượng cao - rô bốt, phần mềm, dịch vụ - trong sách trắng này, KUKA hiện cung cấp các công thức nấu ăn đảm bảo thành công cho toàn bộ chuỗi quy trình. Từ giao hàng đến phân phối, cho nhiều ngành công nghiệp khác nhau. Tám ví dụ thực tế cung cấp một cái nhìn sâu sắc ấn tượng.

Khám phá các giải pháp tự động hóa mà mọi người đều thích.

Tải sách trắng

Bạn cũng có thể quan tâm đến