Válassza ki a helyét:

Helyszín

Automated soldering ensures maximum precision and reduces production times

The robot-based soldering solution from ALNEA Sp. z.o.o in Poland reduces production time by 50 percent

2016. február 19.


Robot-based soldering process to ensure compliance with international standards


The soldering process used in so-called through-hole technology (THT) requires the utmost precision. The small structures and the close proximity of components that must not be wetted leave no room for error. With THT, repair processes are time- and cost-intensive, often not reproducible and in some cases not even allowed. “A reliably controlled selective soldering process is the decisive first step on the path to zero-error production for our customers,” explains Krzysztof Kamiński, President of ALNEA Sp. Z.o.o.

New soldering controller now meets international standards


New soldering controller now meets international standards. The ALNEA-ZEUS controller developed by ALNEA was in need of a major update to ensure that it could continue to meet the standards set in the future by the international association of the printed circuit and electronics industries (IPC). The new version of the soldering controller can now access all process parameters, such as the provision of relevant materials for the soldering process, their exact positioning and the prevention of solder spatter outside the work area. 

KUKA small robot supports zero-error production in the selective soldering process

 

The KUKA  KR 6 R900 sixx small robot from the KR AGILUS series precisely meets the requirements placed on it by the selective soldering process.  With a payload of up to 6 kg and a maximum reach of 900 mm, the robot achieves a repeatability of less than ±0.03 mm and is thus ideally suited to the requirements of the soldering process. At ALNEA, it controls the motions of the soldering iron and also holds the board in a fixed position. Thanks to the robotic automation solution, all parameters of the selective soldering process can be monitored reliably via the teach pendant. Furthermore, all data provided by the KUKA robot are fed into the system and used. This has led not only to a noticeable reduction of errors, but also to a significant increase in productivity.