![Industriële automatisatie](/-/media/kuka-corporate/images/industries/case-studies/avt_seabridge/vollers-kuka-2.jpg?rev=754a7de6bb984117b063a86aff3c97b1&w=1900&hash=ABC914A3E977D136BFBB4E1164B00762)
KUKA robot performs quality checks
Official KUKA System Partner AVT Europe developed a tailor-made solution for Seabridge for taking samples from coffee bags. A KUKA KR 22 R1610 robot was used for this.
A solution tailored to the customer
Seabridge came into contact with Official KUKA System Partner AVT Europe from Essen. They quickly understood the problem and came up with a tailor-made solution for Seabridge. AVT Europe developed an industrial automation solution using a KUKA KR 22 R1610 robot from the KR CYBERTECH family with a custom made sample pricker mounted on it. This allows the robot to take a sample of every coffee bag that passes by. This sample is then poured into a sample collector and a quality analysis can take place.
![Industriële automatisatie](/-/media/kuka-corporate/images/industries/case-studies/avt_seabridge/seabridge-kuka-3.jpg?rev=118b680f3f3c43bba0b4e1aa083303e0&w=1400&hash=D0089BBE898B4E0D61EA43A88B7B8B8B)
Before setting up the installation at Seabridge, AVT Europe decided to first test their entire solution internally at their own site. This way they could perfect the installation down to the smallest details and deliver an installation to Seabridge that met their expectations 100%. The installation at Seabridge itself was also completely flawless. AVT Europe perfectly kept to the agreed time frame to install the installation at Seabridge. They carried out the installation, the connectivity and the programming of the KUKA robot completely according to the agreements made. As a result, production at Seabridge was only at a downtime for a minimum period of time. This was an important condition for Seabridge, while a longer downtime would entail higher costs. Because of AVT Europe's professional approach, these costs could be kept to a minimum.
Automation benefits for Seabridge
For Seabridge, this industrial automation solution from AVT Europe brought numerous advantages. They are now able to take a flexible sample of 20% to 100% of the incoming bags without having to compromise on production time. Because the samples are taken by a KUKA robot, each sample is representative time after time. The chance of errors in comparison of manually taken samples has therefore also become non-existent. The KUKA robot also ensures that this process is safer, which is better for the working environment at Seabridge.
![Industriële automatisatie](/-/media/kuka-corporate/images/industries/case-studies/avt_seabridge/vollers-kuka.jpg?rev=042345b9777545759e9e39dad01b9606&w=1400&hash=7F6BB3B5387C7C036A204307978C03C9)
AVT Europe: a reliable partner
Seabridge is therefore more than satisfied with the industrial automation solution developed by AVT Europe. According to Seabridge, AVT Europe has the required know-how and works with an enthusiastic group of employees. AVT Europe listens to the customer and creates a tailor-made solution. They are a partner you can trust.
![](/-/media/kuka-corporate/images/about-kuka/standorte-teaser.jpg?rev=-1&w=1400&hash=46DE3118EE6D164AB6D1C616952D0D0B)