Robot control from the cloud
The companies robomotion GmbH and SOTEC Software Entwicklungs GmbH would like to make the cloud more accessible to a greater public. To achieve this, a robot application has been developed which can be controlled with a smartphone. This application features the new KR 3 AGILUS robot from KUKA.
24 mai 2017
Robot control as a direct experience
“Together with the company SOTEC Software Entwicklungs GmbH, we have developed a means of controlling the robot which does not involve a physical programmable logic controller, as usual, but rather works from the cloud,” explains Dr. Andreas Wolf, CEO of robomotion GmbH. As a result, the installed KR 3 AGILUS robot from KUKA can be controlled with the user’s own smartphone. The application is used at trade fairs and events and is designed to demonstrate the advantages of the cloud to interested parties.