![](/-/media/kuka-corporate/images/press/news/2020/11/robogym/kuka_robot_robogym.jpg?rev=-1&w=1900&hash=118A4ABF94BA6C14592AF3F13B607994)
RoboGym: revolutionary training – not just for top athletes
What does the future of training look like? Can a robot be used for strength training to potentially achieve greater progress? To what extent is there acceptance of technology among the general population and among athletes?
November 16, 2020
![](/-/media/kuka-corporate/images/press/news/2020/11/robogym/robogym_2020_2.jpg?rev=-1&w=1900&hash=1FEF3F18BFA144B20073AB793ADE528B)
The advantages of the RoboGym
Safe and versatile
So far, the RoboGym supports three types of training. In addition to the leg press, there is a knee extension option as well as a rowing exercise for the upper body. The data are displayed on the screen in real time and saved in a Cloud. Upon activating the device, the data are called directly from anywhere in the world and the device adjusts to the height and desired training weight. The acquisition of the data enables significantly more precise screening in which the force actually applied as well as the movements during each part of the exercise can be seen even more precisely. This allows training to be adapted to individual requirements.
![](/-/media/kuka-corporate/images/press/news/2020/11/robogym/robogym_2020_11.jpg?rev=-1&w=1400&hash=0F3902FA36DDF498B9531B3F5FE020C8)
![](/-/media/kuka-corporate/images/press/news/2020/11/robogym/martin_foto-quadrat.jpg?rev=-1&w=250&hash=6B9C01AB07330237949833E2DA927F3D)
Our dream is for the RoboGym to become the standard in professional sports and rehabilitation, and to be found in every Olympic training facility.