Life Science Robotics: Mobilizing bedridden patients with ROBERT®
ROBERT® is an innovative robot that assists with the rehabilitation of bedridden patients. The user-friendly system helps get patients mobilized efficiently and at an early stage, thus relieving medical personnel of physically strenuous work. Considering the fact that the system's main component is an LBR Med, ROBERT® is the first robot in the world to be developed specifically for these rehabilitation purposes.
ROBERT® is a class IIa medical product, is CE-certified in accordance with the Medical Product Directive (93/42/EEC) and is used in hospitals, care centers and rehabilitation centers. The system can perform the exact exercises created by medical personnel and can be adapted to the specific treatment requirements of each new patient.