Select your location:

Location

Select your language:

  • English
  • English
  • English
  • English
  • Swedish
  • English

Green inovated technology developed by Amatec A/S for RoadTech A/S

Smart automation that effectively saves time, environment and manpower

28 September 2021


KR Cybertech is part of the teamwork

RoadTech has together with KUKA's partner Amatec developed an brilliant solution. A fully automatic machine that easily is screwing down roadmarks that are automatically placed without stop in the ground, along the road. Everything is done automatically while driving and the truck continuously rolls forward without stopping, which leads to a lower environmental impact and time savning. The machine has double capacity compared to previous solutions on the market, this also provides increased traffic safety for both operator and other users of the road. KUKA´s CYBERTECH robot supplies the feed of sticks to the tool.

Green inovated technology developed by Amatec A/S for RoadTech A/S

00:00
00:00
RoadTech's recyclable screwdriver is an extra reinforced stick that is screwed into the ground. It is a unique patented screw, and it is tested by the Norwegian road administration. It 4x as fast as today's plow sticks. The roadmarks are also recyclable and broken sticks are used to make new sticks! 
GPS and data collection from the work operation is central and gives contractors the opportunity for continuous improvement.  Smart automation that effectively saves time, environment and manpower